Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
A clean energy solution with igus on board22-10-14

Automated docking of a floating power plant in the Hamburg harbour reduces emissions

The “Hummel” LNG HYBRID barge was baptised in a ceremony in Hamburg’s Hafencity. Cruise ships can now be supplied with power whilst in port, thanks to the use of this floating LNG power plant. It uses environmentally-friendly liquefied natural gas – LNG. This saves fuel and reduces cruise ships’ emissions. The coupling process takes place at the dock using a complete solution from the switching cabinet to the connectors.


Normally, the ships’ own on-board generators continue to run in order to supply the cruise ships with electricity during their time in port. Becker Marine Systems designed and built the “Hummel” HYBRID LNG barge for the Port of Hamburg in order to reduce pollution in the future. Hummel is a floating LNG power plant which supplies cruise liners with electrical power. The leading energy supply experts at igus were brought into the project in order to deliver the energy from the barge to the docks, where they are then connected to cruise ships. igus is used to providing customised solutions, but this was a new case as all the electronics and steel structures were designed and supplied by igus.

Automatic connection
As soon as the barge arrives at its berth, a gangway moves out, connecting staff on board with the shore. Energy chains from igus are underneath this gangway carrying four thick 6-10kV cables with connectors. These are connected to large power supply boxes as soon as the gangway is docked and the chains are connected. The system connecting the barge must also compensate for the constant motion due to waves and tidal fluctuations. The barge will come into regular use for the 2015 cruise season.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH