Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.

Mon interlocuteur
Sélectionner un site

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

BE(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ?

Articles de presse par domaine

Record-low costs and sustainability: our new slewing ring bearing30-08-23

igus is adding a ready-to-install low-cost variant made from regranulated high-performance plastics to its iglidur PRT series

It is affordable, compact, lightweight and ready to install with a mouse click: igus has added a minimalist low-cost variant to the portfolio of its iglidur PRT series of slewing ring bearings. The PRT-05-15-PC not only reduces costs, but also protects the environment. The new slewing ring bearing consists of 97% regranulated high-performance plastics.


From packaging machine to assembly line to operating table: slewing ring bearings are used in a large number of rotary movements around a fixed axis. However, for many bearing points with low loads, such as those found in furniture construction or display technology, the bearings are often oversized and too expensive. Therefore, such applications often contain metal ball bearings. The problem is that the rolling bearings often take up a great deal of space and require assembly work because they often need fitting. They are also maintenance-intensive as they require continuous lubrication to function. "To eliminate these disadvantages, we decided to add a ready-to-install, low-cost variant to our slewing ring bearing portfolio," says Marc Trenkler, iglidur PRT Product Manager at igus. "So far, there have been hardly any ready-to-install, relatively inexpensive slewing ring bearings on the market," says Trenkler.

Minimalist design reduces required installation space, weight and costs
The new low-cost slewing ring bearing design follows minimalist principles. "Our goal was to produce a light, compact, ready-to-install bearing with as few components as possible," says Trenkler. The PRT-05-15-PC consists of just an inner ring and an outer ring, which slide over each other without balls. It is manufactured in a cost-effective injection-moulding process entirely from lightweight high-performance plastic - without an ounce of metal. It has a diameter of 100 millimetres, is only ten millimetres high and weighs 72 grammes. The reduced complexity makes the new low-cost slewing ring bearing not only compact and lightweight, but also quick to assemble. "Our employees only have to put the inner and outer ring together with a clip bearing. This allows us to offer the bearing to our customers at low cost," says Trenkler.

Low-cost slewing ring bearing made of 97% regranulate
The PRT-05-15-PC not only reduces costs, but also protects the environment. The new low-cost slewing ring bearing has a 97% content of regranulated iglidur M260 and iglidur P4 high-performance plastics. These are materials, such as production sprue, that have already been processed. Valuable plastics are thus saved from incineration and transferred to a sustainable circular economy. The plastic also has microscopic integrated solid lubricants that are released during operation and allow low-friction dry operation without lubricating grease for an additional environmentally friendly effect, which is a great advantage. Every year, millions of tons of lubricants pollute the environment. Finally, the new PRT is durable, especially outdoors. The polymer bearings do not corrode and are resistant to contamination from grease and dirt. This means that they don't have to be replaced as often. "The iglidur PRT-05-15-PC thus contributes to the EU sustainability strategy," says Trenkler. That strategy is aimed at making Europe the first climate-neutral continent by 2050 while boosting economic growth.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH