Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Even more reliability over long travels thanks to the new igus i.Sense EC.B rope hoist sensor for e-chains23-09-22

One instead of two: condition monitoring for chains of 35 metres or more now with a single sensor

Loads, high speeds and the most adverse environmental conditions: energy chains often have to withstand severe stresses. Safe cable guidance is a challenge, e.g. for very long travels like those in large crane systems. To ensure even greater system safety in such cases, igus now offers users the i.Sense EC.B with a new rope hoist sensor for intelligent condition monitoring for chains of 35 metres or more.


Snow, ice, dirt, foreign bodies or a bent trough: there are a wide variety of external influences that can cause even the most robust, durable energy chain to break during operation. In order to avoid unplanned downtimes and the associated costs, the motion plastics specialist igus offers users the proven i.Sense EC.B system for e-chain condition monitoring. Potential chain breaks can be detected in a flash, even on very long travels. The new rope hoist sensor means that only a single sensor is now required for intelligent condition monitoring for chains of 35 metres or more. The measurement range extension from 80 to 999 millimetres eliminates the need for the second sensor on the fixed end side. The longer measurement path also offers better precision over long travels. If breakage is detected, the sensor immediately triggers a message, and the evaluation module sends a signal to the system's control unit. Two sensors (for reverse systems, for example) can also be connected to the new i.Sense GEN II evaluation module. If they are connected to the control system's digital I/O ports, they can also be used to trigger a rapid system shutdown. The new rope hoist sensor is compatible with all previously delivered EC.B systems and i.Sense modules, and can also be integrated into IIoT concepts.

Resistant to weather effects
The igus i.Sense system has already proven itself in many industries, e.g. in very dynamic applications in the automotive sector. But Industry 4.0 is increasing demands on machines and monitoring systems - as crane systems show. Cranes are working faster and faster as travel distances get longer and longer. This makes a robust, durable energy supply system that much more important. "We want crane operators to benefit from the positive i.Sense EC.B system experiences in the automotive industry," says Richard Habering, Head of Business Unit smart plastics at igus. "For safe, failure-free handling of lots of heavy cables in adverse environmental conditions, real-time status detection along the entire travel adds immense value for port or crane operators." In addition to the longer measuring distance, the new rope hoist sensor is characterised by extreme weather resistance and robustness, making it especially interesting for outdoor applications. Fully automated crane systems are particularly susceptible to unexpected downtimes because there is no driver to hear any warning signals. For optimum protection against unexpected failures, crane operators can use the reliable i.Sense EC.B monitoring system instead.

More reliability, lower costs
The igus smart system gives customers full control, a good overview and a reliable energy supply. This extends the service life of both the energy chain and the machine on which it is used. igus conducts ongoing test series in the industry's largest test laboratory for dynamic power transmission systems to continuously optimise the longevity of its motion plastics products. Early system failure warnings from the i.Sense EC.B system also greatly reduce costs: acquisition costs are lower, since only one sensor is required for real-time condition monitoring for chains of 35 metres or more, and maintenance costs can be reduced. Instead of maintaining their systems at regular intervals, companies can perform condition-based maintenance, avoiding unnecessary or early chain replacement.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH