Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Real-time monitoring is more affordable than ever: igus service life sensor starts at 248 euros20-07-22

The new i.Sense EC.W sensor allows cost-effective real-time condition monitoring for gliding e-chain systems

Machine failures and downtimes are among the biggest cost drivers in industry. So it is important for maintenance personnel to prevent unplanned downtime. With the new low-cost service life sensor from igus, users can now make their e-chain smart from as little as 248 euros. Thanks to real-time condition monitoring, maintenance over the entire service life is more predictable, easier and cheaper. This not only brings decisive advantages in the area of e-chains but also offers new possibilities for condition monitoring in many other wear applications.

br> Internet of Things, Big Data, and autonomous robots: The transition to Industry 4.0 is in full swing. This also applies to components that work in machines and have long since become smart, for example by providing data on their condition. However, the integration of smart technologies is often complex for companies and involves external installation work. “We have also found that while online services are very popular in everyday private life, the sensitivity to external data connections is very high in the business environment. The IoT connection of a machine is often not wanted. However, the customer does not want to do without smart functionalities and the integration into existing control systems,” explains Richard Habering, Head of the igus smart plastics Business Unit. This is exactly where igus comes in with the new i.Sense EC.W service life sensor for gliding e-chain systems. The low-cost sensor product allows cost-effective real-time wear detection from as little as 248 euros and thanks to integrated potential-free contacts, can be connected directly to the PLC machine control system without an internet connection. The sensor, cable and evaluation electronics are included. Users also have the option of connecting the sensor to a variety of networks and IoT systems via the i.Cee module and thus integrating it into a predictive maintenance concept. The service life sensor is available for the E4.32, E4.42, E4.56 and E4.80 igus e-chains – more sizes for the E4Q, E2.1, and E2/000 series are already being planned.

Determine service life quickly and easily – and even remotely
The basic principle of the new low-cost sensor system is simple: Conductive elements are incorporated into the high-performance polymers of almost all igus products at the tribologically stressed areas. Clever geometric positioning of these elements allows clear statements to be made about the product service life in the event of an electrical interruption or a change in resistance. This information can simply be output to the operator via the system monitor and, for example, when the 25 percent level is reached, linked to the information about the pending chain replacement. The i.Sense EC.W sensor offers considerable added value, especially for harsh, dark, and dirty environments and highly frequented or hard-to-reach applications. It is mounted on the last crossbar on the fixed end side and records the current state of the chain's side sections. The sensor measures the distance between the crossbars, which narrows in proportion to e-chain side section abrasion. The sensor can therefore be used to monitor each machine wear part remotely – which could benefit many other motion plastics in the future.

Reduce costs by 80% with plannable maintenance
Condition-based alarm messages can prevent unplanned downtimes or unnecessary or premature chain replacement – which also offers an advantage in terms of sustainability. This means that e-chains are no longer replaced according to maintenance intervals, but only when necessary – ultimately reducing maintenance costs as well. Connecting the service life sensor directly to the plant control system can reduce costs by up to 80%. To ensure the best possible product quality, igus performs numerous tests in the test laboratory. More than three billion test cycles are recorded and analysed each year for energy chains alone. These tests are used to continuously optimise and refine igus products. For example, the development engineers have greatly reduced the size of the service life sensor to 2.5mm x 4mm so that measurements can be carried out at other points as well and clear status information generated for almost all gliding applications. In conjunction with the igus service life calculators, potential is therefore unlimited.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH