Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
A clean performance: igus wins the REINER! Award for modular cleanroom chain27-05-21

Fraunhofer Purity Technology Award goes to the particle-free and compact e-skin flat energy supply system

High-purity manufacturing environments ensure that electronics also function safely in everyday life. In order for manufacturers to produce in cleanrooms, particle-free machine elements are required. Every year, the Fraunhofer Institute honours the most innovative developments with the REINER! Award. The motion plastics specialist igus is very pleased with the 2nd place award for its e-skin flat energy supply chain. The alternative to the flat belt guide is compact, modular and has cleanroom class 1. The cables can be easily inserted into the chain using the zipper principle and can be quickly replaced in the event of maintenance.

Microchips, flat screens, implants, active pharmaceutical ingredients or micro and nano products would be unthinkable without high-purity manufacturing environments. Memory ICs are very much in demand, especially in home offices, in expanded corporate IT infrastructures and in medical electronics. At the same time, manufacturers are looking for machines and systems that work quickly and safely to meet the growing demand for semiconductors. One of the biggest challenges here is particles that detach from machine elements and contaminate the ambient air. Therefore, new solutions are required that make the production processes economical, even under high safety and hygiene requirements. To honour these new developments, Fraunhofer IPA announces the Fraunhofer Purity Technology Prize REINER! every two years. The award has now been presented to igus for the development of the e-skin flat energy supply system as part of the Digital 365 Cleanroom Process. The motion plastics specialist took 2nd place.

e-skin flat: modular and compact cable guidance system
The e-skin flat is a modular cable guidance system made of high-performance polymer, which shows almost no visible wear and is abrasion-resistant. Energy supply systems can be easily extended with so-called "single pod" profiles. A zipper system allows easy replacement of the cables. In combination with CFCLEAN cable cores for the transmission of energy, motor control, bus and Ethernet signals, the user receives a ready-to-connect energy supply system. Tests by the Fraunhofer Institute for Manufacturing Engineering and Automation IPA have shown that the system achieves Class 1 according to ISO 14644. This means that the e-skin flat meets the strictest cleanroom requirements. The igus range of particle-free energy supply systems has been in production since 2003. Since last year, the company has also been operating a cleanroom laboratory for in-house development, which was installed at the main site in Cologne in co-operation with the Fraunhofer Institute. In this laboratory, igus tests its e-skin flat as well as other motion plastics such as cables and plain bearings.

You can find more information about the e-skin flat at:
https://www.igus.in/info/e-skin-flat


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH