Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Lubrication-free adjustment: polymer rollers assist igus' hybrid linear system17-04-20

Hybrid roller bearing with tribo-polymer sliders halves coefficient of friction in lateral position

In order to move doors, monitors or even panels, users rely on lateral installation of the linear systems. To enable the linear guides to absorb these lateral forces better, igus has now developed a new hybrid linear system. Two hybrid bearings provide low-friction adjustment with polymer rollers and tribo-polymer slide elements. Combined with an easily fit rail adapted to the new roller bearings, igus offers a cost-effective and visually appealing complete solution.


In the packaging industry, furniture technology or even in machine tools: drylin linear guides can be found wherever movement is required. On tribologically optimised liners, the linear carriages slide on the rail, ensuring precise and long-lasting adjustment. If a low driving force is required for manual adjustments, rollers are used in the bearing element. Especially for a lateral installation, the position of the rollers for the force absorption is crucial. As a solution for such applications, igus has now developed two new hybrid roller bearings, which offer smooth adjustment with low drive forces and maximum support at the same time. The WJRM-41-10 has two offset polymer rollers with optimised alignment for better force absorption and easier rolling. The hybrid roller bearing WJRM-31-10 with single roller is in turn the matching, supporting bearing on the opposite side. By using the two roller bearings, the user can minimise the coefficient of friction by half and increase the service life of the application. In both bearings, in addition to the rollers, there are sliding elements made of the low-friction tribo-polymer iglidur J. The lubrication-free and maintenance-free material is characterised primarily by its low coefficient of friction in dry operation. Both bearings can be positioned at the desired bearing clearance. These are very cost-effective if the bearings are produced in the zinc die-casting process.

Smooth adjustments with low-friction
Using a top plate, the two new roller bearings can be expanded to a linear carriage. To ensure that the bearings can also be used on the appropriate guide, igus has developed a low-profile hybrid roller rail. This has a special geometry optimised for the hybrid roller bearing. The rail has a simple design without visible holes and is able to attach from the back with sliding blocks. This makes the new rail in combination with the hybrid roller bearing ideal for lateral installation, for example in kitchen and furniture construction as well as in machine tools or in jig construction.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH