Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.
Presse |
|
Vous avez des questions ? Vous avez besoin de documentation ? Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger. Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax ! |
|
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ? |
e-chain expert: ready-to-connect energy supply system easily configured online09-06-19
The quick way to a ready-to-connect energy chain is made even easier with the igus e-chain expert. With the aid of the new free-of-charge and freely accessible online tool, users can design their energy chain system using a smart phone, tablet or a desktop computer. Whether an unsupported, gliding or hanging application, the configurator determines the energy chain that is optimally suited. To do this, the user simply has to open the e-chain expert (www.igus.eu/e-chain-expert) select the unharnessed or harnessed cables, enter the application and environmental parameters, decide on the appropriate energy chain from a pre-selection and configure it. In the energy chain configurator, the user can choose from over 1,300 highly flexible chainflex cables tested by igus as well as over 4,200 harnessed readycable drive cables. These are tested and, like all igus cables, come with a 36-month guarantee. On the basis of the specified cables and the application data such as installation space, movement and environment of the energy chain, the customer can choose from a selection of 150,000 e-chain parts for the most cost-effective solution. All igus products are tested in our own 3,800 square metre laboratory. |