Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Reliable in wind, waves, and weather: DNV GL certified cables for e-chains24-01-19

Over 370 chainflex cables from igus for a secure and long-lasting energy and data supply at sea

Oil rigs, gas production facilities, wind farms, port facilities or ship cranes: these applications have very special requirements for safe energy and data transmission. The company igus is the only manufacturer to develop, test and certify cables in accordance with DNV GL for use in maritime e-chains. Today, customers have access to more than 370 control, servo, motor and robot cables as well as bus, data, encoder and fibre optic cables for the safe operation of maritime applications.

The oceans have long been part of the global economy by way of wind farms and worldwide cargo traffic. Offshore companies face similar challenges as their onshore counterparts. For example, in the exploration and transport of raw materials at sea, cost pressure has risen sharply in recent years, so that the automation, which is already state of the art on land today, is also becoming important in the offshore sector. chainflex cables from igus help companies to guarantee the necessary energy and data supply, thereby offering significant cost savings. This starts with straightforward planning using the approved cables, continues with simple installation and ends with smooth and maintenance-free operation in extreme conditions.

Resistant to oil, sun and seawater
Offshore companies and their suppliers who are thinking of expanding their renewable technologies or preparing their merchant fleets for the future, now have more than 370 DNV GL certified cables available from igus. These are designed for the highly dynamic use in energy chains for safe operation at sea. Together with the DNV GL, igus has developed completely new test methods and standards for dynamically used cables in e-chains. In addition to the extensive testing procedures in accordance with DNV GL, the cables have also been tested under real conditions in the igus test laboratory spread over an area of 2,750 square metres. They therefore have a unique guarantee for up to 10 million strokes in energy chains, are flexible in terms of operating temperatures down to -40°C and are also UV-resistant. Besides having seawater resistance, the cables also operate reliably under the influence of oil. The cables are resistant according to MUD NEK606, which enables maintenance-free pumping on drilling rigs and also stands for operator safety. Specially designed for movement in e-chains, the cables reliably carry out their tasks there, regardless of the length of the travel or the load to be moved.

chainflex cables keep maritime installations moving reliably With chainflex cables, plant constructors enjoy maximum freedom for the design of cables and energy chains, since there are virtually no limits to the application areas – whether under water or on the surface, whether under permanent sunshine or in prolonged cold. The use of approved chainflex cables means safe and stable operation of offshore installations for all those responsible for the proper running of a facility in shipyards, equipment suppliers, general contracting or manufacturing companies.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH