Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
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
Showdown in the test lab: plastic ball bearings compete against metal bearings in the salt water test04-07-18

The test winner xiros is up to 60 percent lighter and 40 percent more cost-effective than the metallic version

In Cologne, the company igus operates the world's largest test laboratory for plastics in moving applications. More than 12,000 tribological tests are conducted every year at the motion plastics specialists. These include tests that investigate the use of a wide variety of materials in the most varied environments in real test. This time: xiros flanged ball bearings and metal bearings in salt water. The use of lubrication-free and maintenance-free tribo-plastics enabled the xiros bearing to be completely convincing in the experiment.

The engineers of the igus test laboratory filled a container with saltwater from the sea and heated it to +80 degrees Celsius. Then two bearings were put inside for 120 hours: a classic 2-hole flange bearing made of metal and a xiros flange bearing made of xirodur B180, a high-performance plastic that has been optimised by igus for years in terms of wear and media resistance. Both bearings were not completely covered in the test, but exposed to air in order to trigger the corrosion effect.

Metal bearing begins to corrode after a few hours
The test result spoke clearly in the end. After just a few hours, the metal bearing began to corrode. At the end of the test, significant traces of rust were visible on all bearing components. Unlike the bearing of plastic. The xiros flange ball bearing was unfazed even after 120 hours in the aggressive salt water and high temperatures. There is no colour change and no trace of rust. A clear advantage especially in cleanroom applications and use in food and medical technology, where rust poses a hygiene risk. The xiros ball bearings usually consist of four components: the inner and outer rings as well as the cages made of plastic and the balls made of stainless steel or glass. Unlike metal bearings, the wear-resistant polymer bearings enable a very smooth and hygienic dry operation without a single drop of lubricating oil and are maintenance-free. Their long service life can be easily calculated online. In addition, the plastic bearings are electrically insulating, temperature-resistant from -40 to +80 degrees Celsius, non-magnetic and 60 percent lighter and up to 40 percent more cost-effective than comparable metal bearings. They are suitable for absorbing medium loads and due to their reliability, have been preferred by customers around the world for many years, for example, for use in conveyor belts, labelling, handling and packaging machines as well as in filling machines.


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH