Veuillez sélectionner votre lieu de livraison

Le choix du site pays peut avoir un effet sur différents facteurs tels que le prix, les options de livraison et la disponibilité des produits.
Mon interlocuteur
Sélectionner un site

Indiquez-nous votre code postal, et nous vous dirons aussitôt lequel de nos collaborateurs pourra vous aider.

BE(FR)

Reduce time and costs: Module Connect in automated furniture production

Profile

  • What was needed: failover of the automated production line; quick exchange in case of maintenance or malfunction
  • Requirements: savings through optimisation of cable lengths for dynamic movement and fixed installation; central interface
  • Products: readychain® with Module Connect, ready to connect with e-chain® series 14240, chainflex® CF21.UL, CF5, CAPU.A, CF211, CFPE
  • Industry: furniture production; online shop
  • Success for the customer: quick and easy commissioning thanks to central interface. Minimisation of downtimes when servicing is required: ready-to-connect readychain® system can be replaced in two hours.
About the application:
It is a fully automated production system for tailor-made furniture with connected production lines, such as pallet and accessory storage. Customers can configure individual furniture online and order it directly. The high degree of automation helps reduce production and delivery times to a minimum while fulfilling individual customer requirements.
Module Connect in use

The challenge

As part of optimisations subject to process improvements, the central Module Connect interface was added to the existing readychain® solutions. This greatly simplified handling both for commissioning and for service and revision work, and downtimes have been reduced to a minimum.

It was possible to use existing installation space thanks to the flexible modularity. To connect the numerous cables with one another in a way suitable for industrial purposes, four housings from the existing product range, each with four cable inlets and different contact carriers, were used. From the more than 100 different types of the modular range of insulators from the company Harting, we installed among others
  • Pneumatics
  • Power supply with current load range up to 70A
  • Power supply with current load range up to 16A
  • Earth-core
  • Sub-D
igus harnessed the pin side of the Module Connect interface in the factory and then delivered it to the customer after final testing. Experienced igus assembly workers incorporated the other side of the connectors, the socket side of the Module Connect, into the existing system directly on site. Thanks to this service, it was possible to make optimal use of the tight time frame on the construction site. In addition, igus helps minimise possible sources of error and supplies "everything from a single source". 

Solution

igus worked out the interface solution and planned the on-site conversion in close cooperation with the customer.

Coordinated components, such as the energy chain, the chainflex® cables, the Module Connect interface as well as processing by specialised employees guarantee perfect interaction and a comprehensive set of solutions for the customer. Thanks to the strongly promoted readychain® solution, the focus is always on the customers and their concerns.

The plug-and-play solution provides the special added value with Module Connect, which means that various individual plug-in points were combined into one central one. The ready-to-connect readychain® system with Module Connect as an overall assembly enables the customer to assemble and replace the entire energy supply system without electrotechnical specialists.
Module Connect in use
Module Connect in use


Les termes "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" sont des marques protégées de la société igus® en République fédérale d'Allemagne et le cas échéant à niveau international. Il s'agit ici d'une liste non exhaustive de marques (demandes de marques en cours ou marques déposées par exemple) de la société igus ou de sociétés affiliées à igus en Allemagne, dans l'Union européenne, aux États-Unis et/ou dans d'autres pays ou juridictions.

La société igus® GmbH signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants d'entraînements indiqués sur ce site Web. Les produits proposés par igus® sont des produits de la société igus® GmbH