Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Tech Talks: iglide® bearings

Choosing the Right Bearing Shaft Material

With 17 standard materials and over 1,300 bearings available in over 3,000 dimensions, the iglide® standard range is able to meet the most demanding of requirements. From high temperatures to seawater, from food to automotive - directly find, calculate and order the best possible bearing.

All of our iglide® bearing materials are self-lubricating and maintenance-free. 113 sizes up to shaft diameter, 50mm according to DIN ISO3547. Calculate service life and configure the best material and bearing type according to your specific application and requirements. To learn more about our materials and their properties, view our data sheet. To learn more about all of our iglide® bearings, visit the webpage.

Cost Factors

Reducing costs is an important factor for most companies. The ability to use low-cost shafting heavily depends on the bearings chosen to run on it.

For example, ball bearings require very hard (60HRC or above) and smooth (under 4rms) shafting. Bronze bearings are similar: the shafting must be harder than the bronze material being used.

Because of these requirements, shafting choices are limited and a less expensive shafting material may not be suitable for the application. Plastic bushings offer a few more options because they can run on many different shafts.

igus®' plain bearings are available in a wide variety of polymer blends so you can match the lowest price shaft with a bearing most suited to the application.
iglide® plastic bushings with an aluminum shaft For linear applications, igus® recommends an 8-16rms and in oscillating and rotating applications, depending on the bearing material, a 16-64rms.

erosion damage due to shaft being too smooth

Wear Factors

Aside from the cost factors, there are a number of other things to consider when designing shafting into a bearing system. Many things can affect the performance of the bearings used if they are not taken into consideration.

The direct relationship between coefficients of friction and shaft materials means that: if the shaft is too rough, wear can become a problem. Extremely rough shafting can act like a file and separate small particles of the bearing's surface during movement. When a shaft is too smooth, however, an increase in friction can occur due to the shafting and bearing surfaces adhering to one another. When there is a large difference between static and dynamic friction, alongside adhesion between mating surfaces, stick-slip— characterized by a loud squeaking noise—can become a problem.

Particle Damage & Shafting Materials

Another important consideration is how hard and soft particles can damage bearings and shafts. If particles get in between a bearing and its mating surface, both can suffer from increased wear. Dirt, dust and paper fibers are just some elements that can cause problems. Self-lubricating bearings can eliminate this issue because no grease or oil are on the bearing. This means dirt particles cannot penetrate as easily and damage the bearing and shaft.

There are a number of shafting materials and each can affect the wear of a bearing in different ways. Aluminum, case-hardened steel, stainless steel, and chrome-plated steel are just some of the choices. The hardness and roughness of the shaft material plays an important role. Hard chromed shafts, for example, are very hard, but also smooth.

The wear of igus® ' iglide® plastic bushings are lower on this shaft type than any other. However, because of the little surface roughness, stick-slip issues can become a problem.
wear experiments on aluminum shafts
Stainless steel works well in low-load applications, while corrosion-resistant aluminum, when paired with a corrosion-resistant bearing, is ideal for wet applications or where chemicals are present.

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a soultion based on your specific application and requirements.
Contact an igus® expert now
iglide product manager, Nicole Lang


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302