iglide® plastic bushings - machining, installation, bonding


Table 1.13: Guidelines for machining

Procedure Turning Drilling Milling
Cutting tool HSS HSS HSS
Feed rate 0.05-0.5 0.02-0.3 0.02-0.3
Clearance angle 2-10º 3-16º  2-30º
Rake angle 0-8º 5-30º  0-15º
Cutting
speed [m/min]
100-500 20-200 80-500
mounted bushing Picture 1.21: The mounting is done with a level force.

press fit bushings Figure 1.24: Diagram: Press-fit of the bushings

Machining

iglide® plastic bushings are supplied ready to install. Standard sizes are suitable for most applications, but if the plastic bushing does need machining, the adjacent table shows the standard values.

As far as possible, machining the bearing's sliding surfaces should be avoided, as this usually results in a higher wear rate. iglide® M250 is the exception, as it is highly suitable for secondary machining. With other iglide® plastic bushings, the disadvantages of machining the sliding surface can be counteracted with lubrication during installation.

Installation

iglide® plastic bushings are designed to be press-fit, which means they are manufactured oversized as standard. The inner diameter adjusts only after being pressfit into the proper housing bore with the recommended tolerance. The before-pressfit oversized dimension can be up to 2% of the inner diameter, which ensures a proper pressfit. Axial or radial shifts in the housing are also prevented.

The housing bore should be finished in the recommended tolerance and be smooth, flat, and chamfered as far as possible.

Installation should be completed using an arbor press. This is the most efficient installation method and extremely important for preserving the integrity of the bearing. For example, if you use a hammer, the installation of the bearing might be uneven.

Adhesion

Adhering the bushings is not normally necessary. If the pressfit of the bearing could be lost because of high temperatures, the use of a plastic bushing with high temperature resistance is recommended.

If, however, you plan on securing the bushing using adhesives, testing is necessary. The transfer of successful results from other applications is not possible without additional data.

Useful link



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302