Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Cable carriers above and under water

OpenHydro tidal turbine

This regenerative-energy OpenHydro tidal turbine generates electrical power through the inflow and outflow of water at low and high tide on the coast of the Scottish Orkney Islands. The turbine has a diameter of almost 20 feet. An igus® Series 4040 energy chain cable carrier from the E4/4 range protects the chainflex® continuous-flex motor and signal cables during the lifting and lowering movements of the turbine, while also protecting them against the aggressive ambient conditions. The travel distance amounts to approx. 66 feet in a vertical direction above and under the water with the energy chain cable carrier guided in a steel trough. The vertical travel is transformed into a horizontal travel by turning through 90 degrees. A plastic chain makes any kind of maintenance on the open sea superfluous and was the only suitable solution because a conventional metal chain would not have stood up to the technical, environmental and mechanical demands.


water resistant cable carrier cable carrier above water
cable carrier in water
cable carrier submerged in water

More product information

More applications from different sectors

Useful Links



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302