Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.

Potato Planter: Plastic Bushings Replace Bronze Bearings

Download the PDF version of this application story
A manufacturer of agricultural machinery replaced bronze bearings with iglide® J plastic bushings from igus® to eliminate corrosion and increase lifespan on its potato planter. As a result, the company was able to increase service life by 500-600% and reduce costs by up to 80%.

A planter pick arm was encountering several problems due to the oil-impregnated bronze bushings with graphite plugs used. The pick arm rotates through an arc of 15% at a rate of 12-20 cycles per minute. On the West coast, the bronze bearings were experiencing high wear and premature failure due to very abrasive conditions caused by high levels of volcanic ash in the soil. On the East coast, high salt content in the air caused corrosion and seizure.
plastic bushing
The six-row machine uses 144 bearings, all of which are iglide® J plastic bushings. By switching to iglide® J, the company was able to avoid replacing the bronze bushings two or three times a season. With iglide® J, the planter also has a longer service life, increased reliability, an enhanced technical performance and reduced maintenance costs.

“By replacing the bronze with iglide® J plastic bushings, we increased the lifespan by 500-600% and eliminated the seizing and corrosion issues. iglide® J also costs 70%-80% less than the bronze, has substantially increased reliability and reduced cost downtime. After two years of use, I have yet to find a bearing comparable to it.”
Shop iglide® J sleeve bearings

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!
Contact an igus® expert now
Nicole Lang, iglide Project Manager at igus®


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302